{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to set up ATV212 PID and BACnet?
Issue:
Wants to use the  ATV212 and control with the PID function and with BACnet.

Product Line:
ATV212

Environment:
All Serial numbers

Cause:
N/A

Resolution:
Connect to your Bacnet connector.
Set the parameters below
CMOD = 0 this the default value your PID will be ordering by the terminal input
FMOD =4 the PID reference will be given by the channel communication. The reference is HZ and not %
F829= 4 to select the protocol Bacnet
F360=1 to enable the PID and to select the feedback on VIA.

Because there are a lot of parameters for PID please look at the attached sheet.
For many parameters it is impossible to give a value because that will depend of your application.
These parameters are:
F359,F362,F363,F366,F380.

Schneider Electric Egypt and North East Africa