{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will TwidoSuite software run on a Windows 10 machine?
Issue:
Can TwidoSuite run on Windows 10 ?

Product Line:
Twido, TwidoSuite

Environment:
TwidoSuite

Cause:
Can't get Twidosuite to run on Windows 10.

Resolution:
No. TwidoSuite, Twido is an obsolete product and has been replaced with the M221 and EcoStruxure Machine Exert Basic ( formally TwidoSuite) software that will run on Windows 10. The last version of TwidoSuite is version 2.31.4 and it will run on Windows 7 64 bit. With the Ecostruxure Machine Expert Basic and M221 you can import the old Twido programs into Machine Expert Basic and load program into the M221.

Schneider Electric Egypt and North East Africa