{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Why won't my Lithium-Ion Smart-UPS start when the battery is first connected when there is no utility power to the unit?

Issue:

When you first connect the battery there is a delay before the unit can start on battery with no utility power present.

Product Line:

Smart-UPS

Environment:

SMTL750RM2UC, SMTL1000RM2UC, SMTL1500RM3UC - All Serial Numbers

Cause:

If the UPS is not connected to AC Power, then there will be up to a 1 minute delay between the initial connection of the battery and the UPS being ready to start.

Resolution:

Wait 1 minute before pressing the ON key, or connect the UPS to AC power to eliminate the delay.

Schneider Electric Egypt and North East Africa