Search FAQs
Compatibility of PM5100/PM5300 meter hardware with firmware versions
Product Line
PM5100
PM5300
Environment
Firmware
Resolution
PM5100
PM5300
Environment
Firmware
Resolution
- Firmware revision 2.xx is applicable for PM51/53xx meters with enhanced internal memory.
- Firmware V2.xx revision is applicable for Hardware version B1. Hardware version is indicated on the Meter labels
- Firmware version 2.xx is not compatible with firmware version 1.xx.
- Meters with 1.xx firmware can’t be upgraded with 2.xx firmware.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: