{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Mean time between failures (MTBF) for 140CPU67861 in hours ?
The MTBF figures in hours at different temperature and continuous operation are as follows:

140CPU67861
Mtbf 30° Continuous operation
750944.688

Mtbf 60° Continuous operation
437005.446

Mtbf 85°C Continuous operation
259608.23

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.