{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
0x401e04@vip.ASXDCPMS - failed to write config info to database because 'Register exists but label is empty.'. Will retry in 60s.
There are these kind of messages in the System Log.  There is not new historical logging for those SMPs
 0x401e04@vip.ASXDCPMS - failed to write config info to database because 'Register exists but label is empty.'. Will retry in 60s.
 0x40fc04@vip.ASXDCPMS - failed to write config info to database because 'Register exists but label is empty.'. Will retry in 60s.

Cause 1.
One of the inputs connected to a Datarecorder does not have label. It might be that Label was deleted in Desigenr or the VIP file has been modified with Notepad++. 
In this example, an arithmetic module provides the Datarecorder input.

Resolution1

1. Create a copy of the VIP file located at: 
C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert DC Ed\config\cfg\vip\VIP.ASXDCPMS
2. To identify the Module  with the issue, in this example an arithmetic, open the "vip.cfg" and look for an empy label.  You can use "label = <0>"

In my example:
parent = 0x141c000
name = <15>ART448 Result 1
label = <0>


The above shows that Module arithmetic 448 has the issue.

3. Open the VIP with designer and locate the Arithmetic 448.  Click on Modify settings and set up a value for the label.  If you are not sure what to put there, select the Default label.

Before:



Now should look like this:



4. Save the changes.  

This should solve the issue.


 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.