{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause an AnF or load slipping error on the ATV630 and ATV930 Process Drives?
Issue:
AnF or load slipping error on the ATV630 and ATV930 Process Drives

Product Line:
ATV630 and ATV930 Process Drives

Environment:
All

Cause:
Not following the ramp. The speed feedback doesn't match the speed reference.
The sign of the speed feedback is different from the sign of the reference.
The speed is greater than 10% of the nominal speed (FRS)

Resolution:
• Check the brake feedback and the control circuit.
• Check the mechanical state of the brake.
• Check parameter BCI → brake contact input
• Check parameter BLC → brake assignment.
• Check parameter BRT → brake release time.
• Check parameter BET → brake engage time.

Schneider Electric Egypt and North East Africa