- Cyber security improvements:
- Improve application password strategy (CVE-2018-7790, CVE-2018-7791, CVE-2018-7792)
- Protect against some incorrect Modbus requests (CVE-2018-7789)
- Firmware update tool helps ensure controller is not in RUN state before starting the update. If in RUN state, a confirmation is requested
- When deleting a drive(s) from the IO scanner configuration, the software tests the application for consistency and proposes to remove the deleted drive(s) from the respective function blocks
- User-Defined Function Blocks ( DFB )
- Additional project templates:
- xSample_DataLogging_FB.smbe
- xSample_ModbusTcp_IOScanner.smbe
- xSample_TeSysU_1adv123.smbe
- xSample_User-Defined_FB.smbe
- xSample_User-Defined_Function.smbe
Released for:Schneider Electric Egypt and North East Africa