{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Support BACnet Serial (BACnet MS/TP) in PM5300
Issue
BACnet Support in the PM5300 series.

Product Line
PM5320
PM5340
PM5341
PM5320R

Environment
BACnet Communication

Resolution
The BACnet protocol is implemented only in Ethernet variants of PM53xx series meters. So BACnet MS/TP is not supported in PM53xx series.

PM5320, PM5340 and PM5341 meters do not support BACnet MS/TP (BACNet Serial), these meters support only BACNet IP (over Ethernet)

Schneider Electric Egypt and North East Africa