Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How do we open a PDF file from the Vijeo Designer Runtime ?
If the HMI platform you are using has a Windows Operating System, you can create a script in Vijeo Designer to open a PDF from the inside of Vijeo Designer.

Ensure you have a PDF reader installed.

The following syntax works with Adobe Acrobat Reader and PDFXCView

Sys.createProcess("C:\\Program Files (x86)\\Adobe\\Acrobat Reader DC\\Reader\\AcroRd32.exe", "/A C:\\SEI_XBTGH_QRG.pdf");



Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: