{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What can cause an INF8 or Internal 8 error on the ATV630 and ATV930 Process drives?
Issue:
Getting INF8 or Internal 8 error on the ATV630 and ATV930 Process drives.

Product Line:
ATV630 and ATV930 Process drives

Environment:
All

Cause:
The internal 24vdc power supply is not correct or the 13v, 5v or 24vdc control voltage is not ok.

Resolution:
The supply Power (24V) and Control (13V-5V-24V) are not correct
Priciple
The internal power supplies of the control block are monitored, if one is out of range the INF8 fault occurs.
Remedies
- Check with SoMove which power supply
- Change main control board of the drive.
- Change power board

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.