{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can I find the PME 9.0 upgrade map?
Issue
Need information on the upgrade path for PME 9.0

Product Line
Power Monitoring Expert 9.0

Environment
Power Monitoring Expert Upgrade

Cause
Depending on the version of PME that is being upgraded there may be extra steps that need to be taken during the upgrade, such as upgrading to an intermediate version of PME. The Upgrade Map provides a list of any extra steps or requirements that are needed for either an In-Place or Side-by-Side upgrade.

Resolution
The PME 9.0 Upgrade Map can be downloaded from the following link
http://ecobuilding.schneider-electric.com/search?documentUUID=68038942-a7b0-4a31-a989-d7a3674ff4e2&title=PME+9.0+Upgrade+Map#tab/documents
Attached is a screenshot for the PME 9.0 Upgrade Map
Screenshot of Upgrade Map


Schneider Electric Egypt and North East Africa