{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the recommended SQL live database size limit
Issue
A commonly asked question is, how much should be kept in the live data base

Product Line
Power Monitoring Expert

Environment
Power Monitoring Expert
Microsoft SQL

Cause
It really depends on the customer, on how much data he/she wants to keep and also knowing their server specification (hardware).
They need to keep in mind how to the database's growth will affects the performance of the system based on what they have.

To help better determine this use the following documentation linked below:

Resolution
Power Monitoring Expert Database Growth Calculator
Database Growth Calculation formula
Database Maintenance Recommendations

Once the amount of live data have been decided use the following articles to help with database archiving, trimming, and maintenance
How to trim the PME database
How to set up recurring trims on the PME databases

Schneider Electric Egypt and North East Africa

Attachment(s)
PME 8.2 - User Guide.pdf [2.18 MB]
PME 8.2 Design Guide.pdf [5.81 MB]