{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I simulate an input with Unity Pro?
Issue:
The user needs to be able to simulate a discrete input value changing between 0 and 1.

Product Line:
Unity Pro

Environment:
Online with the PLC or with the Unity Simulator

Cause:
The ability to simulate inputs will aide the user during debug and commissioning

Resolution:
It is possible to simulate discrete input operation in Unity Pro. To accomplish this you simply need to use the "Write_Input_Ebool" block. Place a value of either 1 or 0 on the Write_Input_Ebool input and the address of the input point to be simulated on the output of the block. The Write_Input_Ebool block will work with topological or State RAM addressing.


Schneider Electric Egypt and North East Africa