Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Can we use new Easergy Studio to download current settings and import the same settings instead of S1 Studio in Micom P63x relay ?
Yes ,it is possible to download setting from old device & import to new devise using Easergy studio.
First you need to convert the setting file for the new model (Right click on the setting file then click covert setting file) & please save the same in your local system.
After convert the setting file ,you can add the setting file from Right click of the setting file then click add existing file.
First you need to convert the setting file for the new model (Right click on the setting file then click covert setting file) & please save the same in your local system.
After convert the setting file ,you can add the setting file from Right click of the setting file then click add existing file.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: