Issue
What are the the software and hardware requirements for Citect SCADA 2018?Product Line
Citect SCADAEnvironment
Windows 7, Windows 10, Windows Server 2012 R2Resolution
Please see the attached <<Installation Guide.pdf>> starting in Chapter 4 (page 44).Note that Hardware requirements (CPU) vary depending on the number of the number of I/O per server.
Use the tables starting on page 44 to identify the CPU Benchmark (PassMark) score required.
You can then cross-reference the score with eligible CPUs from a website which reports on tested CPU performance such as https://www.cpubenchmark.net/
Also note that the domain "citect.schneider-electric.com" will redirect you to AVEVA - the brand under Schneider Electric that makes Citect.
For support on all AVEVA products including Citect, go to: https://softwaresupport.aveva.com/