{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the definition of ANSI 30 - Local annunciation?
LED indication on the Sepam front panel
- 2 LEDs indicate the unit operating status:
  • green LED ON: Sepam on
  • red “key” LED: Sepam unavailable (initialization phase or detection of an internal failure)
- 9 yellow LEDs:
  • pre-assigned and identified by standard removable labels
  • the SFT2841 software tool may be used to assign LEDs and personalize labels.
Local annunciation on Sepam’s advanced UMI
Events and alarms may be indicated locally on Sepam’s advanced UMI by:
- messages on the display unit, available in 2 languages:
  • english, factory-set messages, not modifiable
  • local language, according to the version delivered (the language version is chosen when Sepam is set up)
- the lighting up of one of the 9 yellow LEDs, according to the LED assignment, which is set using SFT2841.

Schneider Electric Egypt and North East Africa