Issue:
Drive is running at Low Speed, or 0Hz when scaled to 100% and then runs up to 60Hz or High Speed when at 0%.
Product Line:
All Altivar drives
Environment:
All
Cause:
Incorrect wiring
Resolution:
For the drive to run forward, the Analog inputs are polarity sensitive. The Output, or wiper contact from the drive needs to be on the analog input terminal. If you are seeing the scaling when adjusting from 0-100% then you may just need to swap the +10 and COM wires to change the polarity.
Drive is running at Low Speed, or 0Hz when scaled to 100% and then runs up to 60Hz or High Speed when at 0%.
Product Line:
All Altivar drives
Environment:
All
Cause:
Incorrect wiring
Resolution:
For the drive to run forward, the Analog inputs are polarity sensitive. The Output, or wiper contact from the drive needs to be on the analog input terminal. If you are seeing the scaling when adjusting from 0-100% then you may just need to swap the +10 and COM wires to change the polarity.
Released for:Schneider Electric Egypt and North East Africa