{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can the firmware version of X80 IO modules be accessed from the M580?

Issue
Trying to read the firmware version of Analog and Discrete IO modules using either Unity Pro or DDTs from the M580.

Product line
M580, X80, Unity Pro, Unity Loader

Resolution
There are no means for acquiring the firmware version of the IO modules from either the DDTs or Unity Pro. The only method of querying the firmware version of IO modules is using Unity Loader.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: