{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are there any sample Unity Pro projects available?
Issue
Customer is looking for a sample project to help understand programming.

Product line
Unity Pro

Resolution
We do not provide full application specific sample code. The install of Unity Pro does come with generic demo projects. These projects can be found in the default project path and are named 'demounitypro...'. To locate the project path select 'Tools' -> 'Options' -> 'General' -> 'Paths'.
Attached here are the projects which are provided with Control Expert V15.1.
If prompted for a password when opening any project, it is blank, simply hit OK.

Schneider Electric Egypt and North East Africa

Attachment(s)
demo_ControlExpert_M580Safety.sta [6.52 MB]
demo_ControlExpert_Quantum.xef [310.58 KB]
demo_ControlExpert_Premium.xef [322.82 KB]
demo_ControlExpert_M340.sta [2.32 MB]
demo_ControlExpert_M580.ztx [4.09 KB]
demo_ControlExpert_M580.sta [1.95 MB]
DEMO_CONTROLEXPERT_M580HSBY.ztx [3.75 KB]
demo_ControlExpert_Momentum.zef [50.14 KB]
demo_ControlExpert_m580hsby.sta [3.22 MB]