This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Switches used for load-breaking in SM6 36kV complies to electrical endurance class "E3" to IEC 62271-103,
The switch can break up to 100 breaks at its rated current (Ir) at a power factor of 0.7.
The switch can break up to 100 breaks at its rated current (Ir) at a power factor of 0.7.
Released for:Schneider Electric Egypt and North East Africa