Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the definition of ANSI 78PS - Pole slip?
Protection against loss of synchronism on synchronous 
machines, based on calculated active power.
2 types of operation:
  • tripping according to the equal-area criterion, time-delayed
  • tripping according to power swing (number of active power swings):

*suitable for generators capable of withstanding high electrical and mechanical constraints 

*to be set as a number of rotations.

The 2 types of operation may be used independently or at the same time.

 

Schneider Electric Egypt and North East Africa