Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the definition of ANSI 64G - 100 % stator earth fault?
Protection of generators with earthed neutral against phase-to-earth insulation faults 
in stator windings. This function may be used to protect generators connected to 
step-up transformers
100 % stator earth fault is a combination of two protection functions:
  • ANSI 59N/64G1: neutral voltage displacement, protection of 85 % to 90 % of the stator winding, terminal end.
  • ANSI 27TN/64G2: thrid harmonic undervoltage, protection of 10 % to 20 % of the stator winding, neutral point end.

Schneider Electric Egypt and North East Africa