{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the definition of ANSI 27TN/64G2 - Third harmonic undervoltage?
Protection of generators with earthed neutral against phase-to-earth insulation faults,
by the detection of a reduction of third harmonic residual voltage.
Protects the 10 to 20 % of the stator winding, neutral point end, not protected by the
ANSI 59N/64G1 function, neutral voltage displacement.
Characteristics
  • choice of 2 tripping principles, according to the sensors used:
*fixed third harmonic undervoltage set point
*adaptive neutral and terminal third harmonic voltage comparator set point
  • time-delayed definite time (DT) tripping.

Schneider Electric Egypt and North East Africa