{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How is the ATV340 drive programmed to start stop from terminals and use HMI for speed control?

Issue:

Programming an ATV340 to use the dial of HMI for speed reference and digital input (DI1) for Start/Stop control

Product Line:
Altivar 340, ATV340

Environment:
All

Cause:
Programming setup

Resolution:
In the Main Menu, select Complete Settings, then Command and Reference.
Set [Ref Freq 1 Config] Fr1 to [Ref Freq-Rmt Term] LCC
Set [Control Mode] CHCF = [Separate] SEP
Verify  [Cmd channel 1] CD1 = [Terminals] TER

Schneider Electric Egypt and North East Africa