Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
ION8650 firmware v4.30 or v4.31 continuous reset when using IRIG-B time syncing
Issue
A ION8650 meter running firmware v4.30 or v4.31 using IRIG-B for time sync goes into continual reboots or power cycling.

Product Line
ION8650

Environment
ION8650s at firmware 4.30 or 4.31 using IRIG-B for time sync.

Cause
When the meter is set to IRIG-B in the clock source setting, and a valid timestamp is sent to the meter via IRIG-B hardware, the meter performs a reset.  In some cases, this reset only happens once, and the meter will return to normal operation. However, there are reported cases where the meter will continuously reset when a valid IRIG-B signal is present.

Resolution
The condition has been identified and addressed in firmware update v4.31.1 as stated in the What's new in PowerLogic ION8650 firmware V4.31.1 document.  

The suggested resolution is to update to the current version of the firmware v4.31.2.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: