This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Below selection table gives the fuse rated current based on network (service) voltage and transformer rated power:
Important notes:
Important notes:
- Correct operation of the RM6 is not guaranteed when using fuses from other manufacturers,
- Fuse rating given in A, no overload, – 25°C < Temperature < 40°C),
- Fuse type considers: Fusarc CF and SIBA (1) (General case, IEC 60282-1 standard, IEC 62271-105 (to replace IEC 60420) and DIN 43625 standard),
Released for: Schneider Electric Egypt and North East Africa