{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the HMIDT732 include a cut-out template?
Issue:
What are the cut-out dimensions for the Magelis HMIDT732?

Product Line:
HMIDT732

Resolution:
The HMIDT732 includes a cut-out template / stand. The cut-out dimensions for the HMIDT732 are 383.5 mm x 282.5 mm (+ 1/- 0mm)  Width x Height

Schneider Electric Egypt and North East Africa

Attachment(s)
HMIDT732_Packaging.pdf [257.76 KB]