{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause an SLF3 fault on the Altivar Process Drive?
Issue:
SLF3 fault on the Altivar Process Drive

Product Line:
ATV630 ATV930

Environment:
All serial numbers

Cause:
HMI Lost Communications with the VFD

Resolution:
This is a communication fault between the control board and the graphic display terminal.  This fault can only occur when the start command or the speed reference is processed by the graphical keypad (HMI).
If the communication is interrupted for a short time (2s), the trip message will be displayed.
Check the connection of the graphical keypad.
If remote mounted, verify the cable length does not exceed 20m or 65 ft.
If the graphical keypad is disconnected, reconnect the keypad and power cycle the drive to clear the fault.

Schneider Electric Egypt and North East Africa