{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
The clear button on the popup keypad does not work in Vijeo Designer V6.2 SP6
Issue: When using the popup keypad in Vijeo Designer Runtime version 6.2.6, it is not possible to use the clear button to clear the data entered in the field.

Cause: This issue is caused by a bug in the software that prevents the clear button from performing the correct operation.

Environment: Vijeo Designer Runtime version 6.2.6 Build 39

Resolution: This bug in the software has been resolved in Vijeo Designer V6.2 SP8 (version 6.2.8). Please update your software to this version or the latest to fix this issue.

Schneider Electric Egypt and North East Africa