{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the mounting options for Legacy 784 series relay sockets?
Issue:
Mounting options for Legacy 784 series relay sockets.

Product Line:
Legacy General Purpose Relays

Environment:
784 Series Accessories

Resolution:
Socket part number is 70-784D14-1. It is used for 784XDX relays. Socket is panel mounted. It can be mounted on a DIN rail using an adapter with part# 16-784C. It can also be Flange mounted using part number 16784C1 adapter.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.