{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the 3 states of Visibility in EcoStruxure Operator Terminal Expert and how do I use the "Collapsed" state of Visibility?

Issue
What are the 3 states of Visibility in EcoStruxure Operator Terminal Expert and how do I use the "Collapsed" state of Visibility?
Environment
EcoStruxure Operator Terminal Expert (formerly Vijeo XD) - HMI Configuration Software in Windows

Resolution
The Visibility Animation uses 3 states of an Integer Variable to control the visibility of an object.
When the value is:
0 - the object is Visible
1 - the object is Hidden
2 - the object is Collapsed
In Content Screens of types "Uniform Grid", "Stack Panel" or "Dock Panel", objects can be placed adjacent to each other (stacked, or horizontally like a bookshelf). And when an object's Visibility in the middle is set to "Collapsed", it will disappear and be replaced by the multiple adjacent objects.
Please see the attached sample project and screenshots for a Stacked Panel example (it is zipped in Visibility Sample.zip")
The project name is "Visibility Sample.vxdz".
The project was created in Vijeo XD v3.0.20. You can open the .vxdz project in any version of EcoStruxure Operator Terminal Expert - you will be prompted to upgrade the project.
Steps used to create this project (see numbered screenshots):
1) Create a Content page
2) Select the Container Type as Stacked Panel
3) Create objects in the Stacked Panel Content Page (colored rectangles in this example)
4) Assign an INT variable to each Rectangle object's Visibility Animation - See Variables.PNG
5) Add buttons to control the state of the integers (set to 0, 1, 2 for each INT Variable)
See the 5 Results screenshots for different example states of the stacked rectangles and their corresponding INT values.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa

Attachment(s)

Visibility Example.zipVisibility Example.zip [269.45 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: