Issue:
ATV32 drive showing an OHF fault
Product Line:
Altivar 32
Environment:
All
Cause:
Over heating
Resolution:
OHF [Drive overheat] • Drive temperature too high. • Check the motor load, the drive ventilation and the ambient
temperature. Wait for the drive to cool down before restarting.
Check to see if the fans are running. Drive thermal state of 70% and above should allow the fans to come on.
Under monitoring NON- menu.
THd [Drv.thermal state] % Drive thermal state. 100% = Nominal thermal state, 118% = "OHF" threshold (drive overload).
ATV32 drive showing an OHF fault
Product Line:
Altivar 32
Environment:
All
Cause:
Over heating
Resolution:
OHF [Drive overheat] • Drive temperature too high. • Check the motor load, the drive ventilation and the ambient
temperature. Wait for the drive to cool down before restarting.
Check to see if the fans are running. Drive thermal state of 70% and above should allow the fans to come on.
Under monitoring NON- menu.
THd [Drv.thermal state] % Drive thermal state. 100% = Nominal thermal state, 118% = "OHF" threshold (drive overload).
Released for: Schneider Electric Egypt and North East Africa