{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Schneider offer padlockable selector switches?
Issue:
Selector switch with padlock option

Product Line:
22 mm Push Buttons

Environment:
XB4 Selector Switches

Resolution:
The ZB4 series has padlock option.
See the attached catalog section with various options in 2 and 3 positions selector switches.

Schneider Electric Egypt and North East Africa

Attachment(s)
selector switch padlockable.pdf [123.48 KB]