{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the ATV320 obsolete?
Issue:
ATV320 obsolescence

Product Line:
Altivar 320

Environment:
All model numbers, all serial numbers

Cause:
Obsolescence documentation

Resolution:
The ATV320 is not obsolete.
It is a currently marketed product line, introduced in 2016.
The ATV320 is the functional replacement for the ATV32 and the ATV312, both obsoleted in 2017.

updated Feb 2022


Schneider Electric Egypt and North East Africa