{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do our Altivar Process variable speed drives comply to the ATEX certification with EX de motor type? ATEX manual mentions only type Ex d
The EX "de" motors are similar to EX "d" motors. Except terminal blocks and terminal boxes.
Our drives also comply with EX "de" motors.

The EX "de" means that motors must comply with the standards
- Standard IEC 60079-0 : Equipment – General requirements
- Standard IEC 60079-14 : Electrical apparatus for explosive gas atmosphere
- Standard IEC 60079-1 : Equipment protection for EX "d" motor
- Safety devices in EX applications

Schneider Electric Egypt and North East Africa