Issue:
Dissipated heat rating for ATV930 drives.
Product Line:
Altivar 930
Environment:
All
Cause:
Heat loss
Resolution:
The first value is the power dissipated at a nominal current in the forced-cooled area of the drive. The second value is the power dissipated at nominal current in the naturally cooled area, the value used in case of installation using the flush-mounting kit, separate hot and control part in the cabinet. If the drive is installed in a standard cabinet, the sum of both values is to be taken into account.
Dissipated heat rating for ATV930 drives.
Product Line:
Altivar 930
Environment:
All
Cause:
Heat loss
Resolution:
The first value is the power dissipated at a nominal current in the forced-cooled area of the drive. The second value is the power dissipated at nominal current in the naturally cooled area, the value used in case of installation using the flush-mounting kit, separate hot and control part in the cabinet. If the drive is installed in a standard cabinet, the sum of both values is to be taken into account.