Search FAQs
Is there a Magelis HMI series that is rated for outdoors?
Issue:
Looking for an HMI that is rated for outdoors?
Product Line:
Magelis HMIGTUx series
Resolution:
The Magelis HMIGTUx series (HMIG3x with HMIDT35x, HMIDT65x, HMIDT75x) is rated for outdoor use. The screen is rated at 1000 cd/m2 and is suitable for bright outdoor applications. The range of temperatures that the units can be used in are as follows:
HMIDT35x: -30...65 °C (-22...149 °F)
HMIDT65x: -30...70 °C (-22...158 °F)
HMIDT75x: -20...60 °C (-4...140 °F)
The HMIGTUx series is supported by Vijeo Designer V6.2 SP8
Looking for an HMI that is rated for outdoors?
Product Line:
Magelis HMIGTUx series
Resolution:
The Magelis HMIGTUx series (HMIG3x with HMIDT35x, HMIDT65x, HMIDT75x) is rated for outdoor use. The screen is rated at 1000 cd/m2 and is suitable for bright outdoor applications. The range of temperatures that the units can be used in are as follows:
HMIDT35x: -30...65 °C (-22...149 °F)
HMIDT65x: -30...70 °C (-22...158 °F)
HMIDT75x: -20...60 °C (-4...140 °F)
The HMIGTUx series is supported by Vijeo Designer V6.2 SP8
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: