{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the ATV630 be powered directly to the DC bus?
Issue:
Powering the ATV630 directly from the DC bus.

Product Line:
Altivar 630

Environment:
All

Cause:
Powered by DC voltage directly to the DC bus

Resolution:
No, the ATV630 cannot be powered this way. Moreover, the ATV630 cannot be used in 'bus tying' applications either. The DC bus terminals on the ATV630 are only intended for measurement purposes. These terminals should not be used for powering up the DC bus. Please consider an ATV930 for this type of application.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: