{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

What is the difference between form A and form C relay digital outputs in SmartX controllers?

Form A relay digital output:

Form A digital output means that, outputs are normally open contacts with one common terminal (C) and one normally open terminal (NO). The terminals are isolated from signal ground.

Machine generated alternative text:

Form A digital output internal configuration in DO-FA-12 and DO-FA-12-H I/O modules, for AS-P

Machine generated alternative text:

Form A digital output internal configuration in AS-B and MP-Cs

Form C relay digital output:

The Form C digital outputs are switching contacts with one common terminal (C), one normally open terminal (NO), and one normally closed terminal (NC). The terminals are isolated from signal ground.

Machine generated alternative text:Terminal base +24 v RS-485 O module NO iii- NC

Form C digital output internal configuration in DO-FC-8, DO-FC-8-H, UI-8/DO-FC-4, and UI-8/DO-FC-4-H I/O modules, for AS-P

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: