Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What's the difference between Power Supply (P/N MTN693004 ) and KNX Power Supply (P/N MTN684064)?
1. MTN693004 is a normal 24Vdc power supply (it is not a KNX power supply) that can provide ONLY power to the devices connected to it.
2. MTN684032, MTN684064, MTN683832 and MTN683890 are real 24Vdc "KNX" power supplies that not only provide POWER through their wires to the connected KNX devices but also provide COMMUNICATOIN between these KNX devices through the bus channel.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more