{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How does the GAVD0110 auxiliary contact work?
Issue:
Function of a GAVD0110 auxiliary contact.

Product line:
Tesys GV manual starters

Environment:
Auxiliary contacts

Cause:
Contacts do not appear to be working properly.

Resolution:
The GVAD** can only be installed on left side of product and the GV2 must be in OFF position when mounting.

The GVAD0110 has 2 different contacts
One is fault signaling contact (terminals 95/96) NC contact and the second is only standard auxiliary NO contact (terminals 53/54 ).

Fault signaling defect contact should be always in close position excepted when there is fault on GV2 ( short circuit or overload ) at this time contact open.
This fault signaling defect contact is not related to ON/OFF position of GV2’s but to reset back to NC the device must be switched back to the ON position.

Auxiliary contact report the ON/OFF position of GV2’s.
This Auxiliary NO contact is on Open when GV2 is on OFF position and close when GV2 is ON position.

Schneider Electric Egypt and North East Africa