Search FAQs
How can you set, change or remove the password on the Process drives using the Somove software?
Issue:
Customer wants to reset the password using Somove software.
Product Line:
Somove and Process Drive ATV630 and ATV930.
Environment:
All
Cause:
Reset the password using Somove.
Resolution:
On SoMove, going: Device -> Protection, you have the same features when using keypad`s: Main menu -> 4.Password .
Level1/Level2 corresponds to: PIN1/PIN2.
1. To set the password:
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zrcwQAA&oid=00DA0000000abSm)
2. To change the password:
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zrd1QAA&oid=00DA0000000abSm)
3. To remove password:
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zrd6QAA&oid=00DA0000000abSm)
4. Protecting the SoMove file can be done by File/Project properties:
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zrdBQAQ&oid=00DA0000000abSm)
Customer wants to reset the password using Somove software.
Product Line:
Somove and Process Drive ATV630 and ATV930.
Environment:
All
Cause:
Reset the password using Somove.
Resolution:
On SoMove, going: Device -> Protection, you have the same features when using keypad`s: Main menu -> 4.Password .
Level1/Level2 corresponds to: PIN1/PIN2.
1. To set the password:
2. To change the password:
3. To remove password:
4. Protecting the SoMove file can be done by File/Project properties:
Released for:Schneider Electric Egypt and North East Africa
Explore more
Product:
Explore more
Product: