{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
In EcoStruxure Machine Expert, how do I set up the Gateway for downloading my PLC application to a device with a specific Subnet Mask?

Issue

In EcoStruxure Machine Expert or SoMachine v4.3, how do I set up the Gateway for downloading my PLC application to a device with a specific subnet mask?

Product Line

EcoStruxure Machine Expert, SoMachine v4.3

Environment

Configuration Software for Windows

Resolution

To set up the Machine Expert Gateway to be able to connect to devices with a specific subnet mask (in this example, '255.255.255.0'), follow these steps below:

  1. Run Notepad.exe as Administrator in Windows
  2. From Notepad, open the file "Gateway.cfg" in the SoMachine Gateway folder (default location: "C:\Program Files (x86)\Schneider Electric\EcoStruxure Machine Expert\Tools\Gateway")
    (For SoMachine, the location is "C:\Program Files (x86)\Schneider Electric\SoMachine Software\Tools\Gateway\")
  3. Under the [CmpBlkDrvUdp] section, add the line "itf.0.networkmask=255.255.255.0" (or replace 255.255.255.0 with a subnet mask of your choice)
  4. Save the Gateway.cfg
  5. Restart the Gateway Service from the green "=S=" logo icon on the right side of the Windows taskbar (or restart the Windows Service called 'CoDeSys Gateway V3')

Schneider Electric Egypt and North East Africa