1. Issue
This FAQ describes how to get the display HMI target’s IP address with Vijeo Designer2. Environment
Vijeo Designer 6.23. Resolution
In Vijeo Designer, no system variable can be directly used to get HMI target’s IP address. However, we can use system function getinfostring() to get HMI’s IP address and display during runtime.
Examples (Ethernet 1 IP Address):
Sys.getInfoString(IP_ADDRESS_1)
Sys.getInfoString(IP_ADDRESS)
Note:
- The value displayed by the getInfoString() method is the system information at Startup. That
- getInfoString() always returns an empty string when used in Web Gate.
Released for:Schneider Electric Egypt and North East Africa