{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can an ATV320 be used for Synchronous reluctance motors?

Article available in these languages: Spanish

Issue:
ATV320 with Synchronous reluctance motors.

Product Line:
ATV320

Environment:
All model numbers, all serial numbers

Cause:
NA

Resolution:
No, the ATV320 is not designed for reluctance type synchronous motors.  Only ATV600/900 series and ATV340 drives can be used with reluctance motors. These drives have the control law dedicated to run this kind of motor.

Schneider Electric Egypt and North East Africa