{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause an LFF1 error on the ATV12 drives?
Issue:
LFF1 error on the ATV12 drives

Product Line:
ATV12 drives

Environment:
All

Cause:
AI current loss fault

Resolution:
Detection if:
• Analog input AI1 is configured as
current
• AI1 current scaling parameter of
0% CrL1 page 52 is greater,than 3 mA
• Analog input current is lower than 2 mA

Check for loose connections

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: