1.Issue
In simulation mode, Vijieo Designer can’t read external variable value if driver is MODBUS SLAVE.2.Environment
Issue happens in Vijeo Designer 6.2 SP3~SP10.3.Resolution
The feature is not supported in simulation mode since Vijeo Designer 6.2 SP3 to SP10.It will not impact the runtime when it downloaded to a Target for operation.
4.FAQ Applicable Conditions
FAQ applies to Vijeo Designer 6.2 SP3~SP10.Released for:Schneider Electric Egypt and North East Africa