{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to deal with unexpected Short/Close status of IO digital output during Installation of IO Module (LV434063)?

Possible cause:

Shock and vibration on bistable relays during transit

Affected product:

IO Module (LV434063) with firmware version 3.3.11 and earlier.


Solution 1:

Upgrade IO module to v003.004.005 using EcoStruxure Power Commission (v2.12.0.2007 and later).


Solution 2:

FORCE digital outputs to 1, then FORCE to 0, and then UNFORCE.

Procedure

• Using EcoStruxure Power Commission

  1. Open EcoStruxure Power Commission application software and discover your gateway device.
  2. Click CONNECT.
  3. Select Device Check Up tab and go to I/O Status tab.
  4. Select the respective I/O Module (I/O Module 1 or I/O Module 2) on the left side pane.
  5. Select the check boxes to select all three digital outputs of I/O module.
    • Digital Output 1
    • Digital Output 2
    • Digital Output 3
  6. Click FORCE TO 1.
    • You will be prompted to enter the password to perform this operation.
  7. Enter the password and click CONTINUE.
    • A “Success” message is displayed on the Test Result column.
  8. Select all three digital outputs of same I/O module again.
  9. Click FORCE TO 0.
    • You will be prompted to enter the password again.
  10. Enter the password and click CONTINUE.
    • A “Success” message is displayed on the Test Result column.
  11. Select all three digital outputs of same I/O module again.
  12. Click UNFORCE.
    • You will be prompted to enter the password again.
  13. Enter the password and click CONTINUE.
    • A “Success” message is displayed on the Test Result column.
  14. Refer to the snapshot (attached below) of the EcoStruxure Power Commission.

• Using FDM121 Display Module

  1. Connect FDM121 display modue.
  2. Navigate to Main menu and select Services.
  3. Navigate to I/O Module and select the module (I/O Module 1 or I/O Module 2).
  4. Navigate to Force.
  5. Press OK on Force and navigate to O1, O2, or O3.
  6. Select O1 and press OK.
  7. Select Force to 1 and press OK.
  8. Select YES and press OK.
    Result: You will be prompted to enter the password.
  9. Enter the password and press OK.
    Result: The status changes to 1F, which can be seen in front of O1 in the same screen or in Status menu.
  10. Select Force to 0 and press OK.
  11. Select YES and press OK.
  12. You will be prompted to enter the password.
  13. Enter the password and press OK.
    Result: The status changes to 0F, which can be seen in front of O1 in the same screen or in Status menu.
  14. Select UnForce and press OK.
  15. Repeat steps 6 through 14 to change the status of other digital outputs (O2 and O3) to complete Force to 1, Force to 0, and then UnForce.

Schneider Electric Egypt and North East Africa

Attachment(s)

EPC image.jpgEPC image.jpg [68.72 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: