Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How to flash the firmware of the LXM28 drive
Issue:
How to flash the firmware of the LXM28 drive

Product Line:
LXM28
Lexium 28

Resolution:
To flash the LXM28 drive firmware, the following are needed:
- Latest firmware file (currently V1.70.8). This is a file with the extension *.i00 and can be requested from technical support.
- Firmware Update Tool (latest version is 1.0.2.8) and can also be requested from technical support
- USB to RJ45 cable, part # TCSMCNAM3M002P

> Power the LXM28 drive
Connect the USB-RJ45 cable
> Launch the Firmware Update Tool
> Enter the COM port assigned by Windows to the cable
> Browse the firmware in the "Firmware Path"
> Click on Connect - If successful, this should bring up the drive model and version
> Click on Start and wait

The Flash tool is attached herewith. 

Schneider Electric Egypt and North East Africa

Attachment(s)
Fw Update Tool_1028.zip [188.79 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more